> ## Documentation Index
> Fetch the complete documentation index at: https://motorbridge.seeedstudio.com/llms.txt
> Use this file to discover all available pages before exploring further.

# Robstride parameter tables

# RobStride Runtime Parameter Table

<mintly-toc>
  MotorBridge v0.4.1 uses one unified RobStride runtime parameter table from protocol section 4.
</mintly-toc>

MotorBridge keeps the upper-level RobStride API shape shared across RS models. The active runtime parameter table is the protocol section 4 "read/write single parameter" list in the `0x7005..0x702E` range. Older/manual `0x2000` and `0x3000` function-code fields are not split into per-model high-level tables in v0.4.1.

## Runtime Rules

* Runtime parameter read/write uses communication type 17/18 plus the parameter index below.
* Parameter index is little-endian in `byte[0..2]`; the typed value is little-endian in `byte[4..8]`.
* Parameters that must survive power-cycle require type 22 save after writing. In v0.4.1, `robstride-write-param --store 1` performs write, optional verify, then save.
* RobStride `set_zero_position()` keeps the same upper-level API but now writes `zero_sta(0x7029)=1` behind the scenes so zeroed motors use `-pi..pi`. Use `store_parameters` / `--store 1` to persist it.
* Type 22 save uses payload `01 02 03 04 05 06 07 08` and waits for a RobStride status ACK.

## Communication Types Used

| Type | Name                | Purpose                                 |
| ---: | ------------------- | --------------------------------------- |
|    6 | `SET_ZERO_POSITION` | Set current mechanical position as zero |
|   17 | `READ_PARAMETER`    | Read one parameter by index             |
|   18 | `WRITE_PARAMETER`   | Write one parameter by index            |
|   22 | `SAVE_PARAMETERS`   | Persist parameter changes               |

## Section 4 Parameter List

|    Index | Name              |  Type | Bytes | Unit           | Range / Default                                                       | R/W | Notes                                                                                                                                                                                                |
| -------: | ----------------- | ----: | ----: | -------------- | --------------------------------------------------------------------- | --- | ---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- |
| `0x7005` | `run_mode`        |  `u8` |     1 | enum           | `0` MIT, `1` PP, `2` velocity, `3` current, `5` CSP                   | W/R | Selects the active RobStride control mode before mode-specific command parameters are used.                                                                                                          |
| `0x7006` | `iq_ref`          | `f32` |     4 | A              | `-43..43`, current-mode target                                        | W/R | Effective when `run_mode=3` current mode. Positive/negative direction follows motor firmware convention.                                                                                             |
| `0x700A` | `spd_ref`         | `f32` |     4 | rad/s          | `-20..20`, velocity-mode target                                       | W/R | Effective when `run_mode=2` velocity mode.                                                                                                                                                           |
| `0x700B` | `limit_torque`    | `f32` |     4 | Nm             | `0..60`                                                               | W/R | Torque clamp used by firmware. Keep within the motor/manual limit.                                                                                                                                   |
| `0x7010` | `cur_kp`          | `f32` |     4 | gain           | default `0.17`                                                        | W/R | Current-loop proportional gain. Tune carefully; bad values can destabilize current control.                                                                                                          |
| `0x7011` | `cur_ki`          | `f32` |     4 | gain           | default `0.012`                                                       | W/R | Current-loop integral gain. Tune carefully.                                                                                                                                                          |
| `0x7014` | `cur_filter_gain` | `f32` |     4 | ratio          | `0..1`, default `0.1`                                                 | W/R | Current filter coefficient.                                                                                                                                                                          |
| `0x7016` | `loc_ref`         | `f32` |     4 | rad            | position target                                                       | W/R | Position command used by PP/CSP-style position modes.                                                                                                                                                |
| `0x7017` | `limit_spd`       | `f32` |     4 | rad/s          | `0..20`                                                               | W/R | Position/CSP speed limit. MotorBridge POS\_VEL path writes this before `loc_ref`.                                                                                                                    |
| `0x7018` | `limit_cur`       | `f32` |     4 | A              | `0..43`                                                               | W/R | Current limit for velocity/position modes.                                                                                                                                                           |
| `0x7019` | `mechPos`         | `f32` |     4 | rad            | read-only                                                             | R   | Load-side counted mechanical position. After MotorBridge RobStride zero + store, startup range is intended to be `-pi..pi` via `zero_sta=1`.                                                         |
| `0x701A` | `iqf`             | `f32` |     4 | A              | read-only                                                             | R   | Filtered q-axis current feedback.                                                                                                                                                                    |
| `0x701B` | `mechVel`         | `f32` |     4 | rad/s          | read-only                                                             | R   | Load-side velocity feedback.                                                                                                                                                                         |
| `0x701C` | `VBUS`            | `f32` |     4 | V              | read-only                                                             | R   | DC bus voltage.                                                                                                                                                                                      |
| `0x701E` | `loc_kp`          | `f32` |     4 | gain           | default `60`                                                          | W/R | Position-loop proportional gain.                                                                                                                                                                     |
| `0x701F` | `spd_kp`          | `f32` |     4 | gain           | default `6`                                                           | W/R | Speed-loop proportional gain.                                                                                                                                                                        |
| `0x7020` | `spd_ki`          | `f32` |     4 | gain           | default `0.02`                                                        | W/R | Speed-loop integral gain.                                                                                                                                                                            |
| `0x7021` | `spd_filter_gain` | `f32` |     4 | ratio          | default `0.1`                                                         | W/R | Speed filter coefficient.                                                                                                                                                                            |
| `0x7022` | `acc_rad`         | `f32` |     4 | rad/s^2        | default `20`                                                          | W/R | Velocity-mode acceleration limit.                                                                                                                                                                    |
| `0x7024` | `vel_max`         | `f32` |     4 | rad/s          | default `10`                                                          | W/R | PP mode maximum velocity.                                                                                                                                                                            |
| `0x7025` | `acc_set`         | `f32` |     4 | rad/s^2        | default `10`                                                          | W/R | PP mode acceleration. If deceleration split is enabled in firmware, `dcc_set(0x702E)` may control deceleration separately.                                                                           |
| `0x7026` | `EPScan_time`     | `u16` |     2 | ms step        | default `1`; `1=10 ms`, each +1 adds `5 ms`                           | W   | Active-report interval setting. Only matters when active report is enabled by communication type 24.                                                                                                 |
| `0x7028` | `canTimeout`      | `u32` |     4 | firmware ticks | default `0`; `20000=1 s`                                              | W   | CAN timeout threshold. `0` disables/uses default firmware behavior depending on firmware. Save if persistence is required.                                                                           |
| `0x7029` | `zero_sta`        |  `u8` |     1 | enum           | default `0`; `0=0..2pi`, `1=-pi..pi`                                  | W   | MotorBridge RobStride `set_zero_position()` writes `1` automatically. Use type 22 save / `--store 1` for power-cycle persistence.                                                                    |
| `0x702A` | `damper`          |  `u8` |     1 | switch         | default `0`; `1` cancels power-off back-drive damping                 | W/R | Controls the shutdown/back-drive damping behavior described by the RobStride manual. Save if persistence is required.                                                                                |
| `0x702B` | `add_offset`      | `f32` |     4 | rad            | default `0`                                                           | W/R | Adds an offset to the current zero. Example: after zeroing at physical `1 rad`, setting `add_offset=1` makes that physical position report as `1 rad` after reboot while zero is shifted by `1 rad`. |
| `0x702C` | `alveolous_open`  |  `u8` |     1 | switch         | default `0`; `1` enables cogging compensation                         | W/R | Enable after cogging calibration has succeeded. The manual says calibration should be done unloaded and typically with `iq_test=1`.                                                                  |
| `0x702D` | `iq_test`         |  `u8` |     1 | switch         | default `0`; `1` enables extended initialization/calibration behavior | W/R | Used for motor initialization calibration and as a preparation step for cogging calibration. Save/reboot behavior depends on firmware workflow.                                                      |
| `0x702E` | `dcc_set`         | `f32` |     4 | rad/s^2        | default `10`                                                          | W/R | PP-mode deceleration. The manual notes this is used when PP acceleration/deceleration are separated by firmware configuration.                                                                       |

### Persistence and Zeroing Notes

* `W/R` or `W` only means the parameter can be written over CAN; it does not guarantee persistence by itself. Use `motorbridge-cli robstride-write-param ... --store 1` when a parameter value must survive power cycling. `motorbridge-cli run --vendor robstride ... --mode save` remains available as a direct save operation.
* For RobStride zeroing, MotorBridge keeps the same upper-level command as other vendors. Internally it sends type 6 and then writes `zero_sta(0x7029)=1`; with `--store 1`, type 22 saves the `-pi..pi` startup behavior.
* Use radians for all position quantities and radians per second / radians per second squared for velocity and acceleration.

## Examples

Read `mechPos`:

```bash theme={null}
motorbridge-cli robstride-read-param \
  --channel can0 --model rs-06 --motor-id 2 --feedback-id 0xFD \
  --param-id 0x7019 --type f32
```

Write `damper=1` and save:

```bash theme={null}
motorbridge-cli robstride-write-param \
  --channel can0 --model rs-06 --motor-id 2 --feedback-id 0xFD \
  --param-id 0x702A --type u8 --value 1 --verify 1 --store 1
```

## RobStride Zero Calibration

Use the unified Python package CLI. The current CLI uses subcommands, so
RobStride control commands must start with `motorbridge-cli run`.

Before writing zero:

* Use a verified adapter path, preferably PCAN or a tested CANable/candleLight
  SocketCAN interface.
* Scan first and confirm the target `motor-id` and `feedback-id`.
* Move the joint by hand to the real mechanical zero pose.
* Do not run this command while the mechanism can collide or fall.

Scan and confirm the motor is online:

```bash theme={null}
motorbridge-cli scan \
  --vendor robstride --channel can0 \
  --start-id 1 --end-id 127 \
  --feedback-ids 0xFD,0xFF,0xFE,0x00,0xAA
```

Read state once:

```bash theme={null}
motorbridge-cli run \
  --vendor robstride --channel can0 --model rs-00 \
  --motor-id 1 --feedback-id 0xFD \
  --mode enable --loop 1 --dt-ms 100
```

Set the current mechanical pose as zero. `--zero-exp 1` is required for
RobStride; without it, MotorBridge prints a warning and does not send the
zeroing CAN frame. `--store 1` saves the result when the firmware accepts it.

```bash theme={null}
motorbridge-cli run \
  --vendor robstride --channel can0 --model rs-00 \
  --motor-id 1 --feedback-id 0xFD \
  --mode set-zero --zero-exp 1 --store 1 \
  --loop 1 --dt-ms 100
```

Verify by reading state again:

```bash theme={null}
motorbridge-cli run \
  --vendor robstride --channel can0 --model rs-00 \
  --motor-id 1 --feedback-id 0xFD \
  --mode enable --loop 3 --dt-ms 100
```

Then test a small move and return to zero:

```bash theme={null}
motorbridge-cli run \
  --vendor robstride --channel can0 --model rs-00 \
  --motor-id 1 --feedback-id 0xFD \
  --mode pos-vel --pos 1.5 --vlim 1.0 --loc-kp 5.0 \
  --loop 1 --dt-ms 20

motorbridge-cli run \
  --vendor robstride --channel can0 --model rs-00 \
  --motor-id 1 --feedback-id 0xFD \
  --mode pos-vel --pos -1.5 --vlim 1.0 --loc-kp 5.0 \
  --loop 1 --dt-ms 20
```

For RobStride, MotorBridge also writes `zero_sta=1` internally so the startup
range is intended to be `-pi..pi`. Use the model that matches your motor for
limits and logging; the examples above use `rs-00`.