Skip to main content

API: Motor

Import

Class Overview

Motor instances are created by Controller.add_*_motor() methods. Do not instantiate directly.

Lifecycle Methods

close()

Release motor handle resources. Called automatically when controller closes. Parameters: None Returns: None Example:

enable()

Enable motor output (apply power to windings). Parameters: None Returns: None Raises: CallError on failure Example:

disable()

Disable motor output (release power, motor becomes free-spinning). Parameters: None Returns: None Raises: CallError on failure Example:

clear_error()

Clear any error state on the motor. Parameters: None Returns: None Raises: CallError on failure Example:

set_zero_position()

Set current position as zero reference point. Parameters: None Returns: None Raises: CallError on failure
This modifies motor’s internal position reference. Use with caution in multi-motor systems.
Example:

Mode Control

ensure_mode(mode, timeout_ms=1000)

Switch motor to specified control mode with timeout. Parameters: Returns: None Raises: CallError if mode switch fails or times out Example:

Control Commands

send_mit(pos, vel, kp, kd, tau)

Send MIT mode control command. Provides full control over position, velocity, stiffness, damping, and torque. Parameters: Returns: None Raises: CallError on failure Example:
MyActuator does not support MIT mode. RobStride has limited MIT support.

send_pos_vel(pos, vlim)

Send position-velocity mode command. Motor moves to position with velocity limit. Parameters: Returns: None Raises: CallError on failure Example:
RobStride supports POS_VEL mode. A vlim of 0 skips the limit_spd (0x7017) write, so the motor keeps its last set velocity limit; only loc_ref (0x7016) is written. Pass a non-zero vlim to update the limit. PP/CSP variants robstride_send_pos_vel_pp / robstride_send_pos_vel_csp follow the vendor manual PP/CSP sequences and apply the same > 0 guard to their velocity/acceleration registers; for high-rate loops use a prepared profile and write loc_ref directly each cycle.

robstride_send_pos_vel_pp(pos, vel_max, acc_set) (RobStride)

Send RobStride PP (Profile Position) mode command. Motor moves to the target position via a profiled trajectory. Parameters: Returns: None Raises: CallError on failure Example:

robstride_send_pos_vel_csp(pos, vlim) (RobStride)

Send RobStride CSP (Cyclic Synchronous Position) mode command. Motor cyclically tracks the target position each cycle. Parameters: Returns: None Raises: CallError on failure Example:
PP and CSP both write the position target to loc_ref (0x7016), but their velocity/acceleration registers differ: PP writes vel_max (0x7024) + acc_set (0x7025); CSP writes limit_spd (0x7017). The modes also differ: PP uses run_mode=1, CSP uses run_mode=5.

send_vel(vel)

Send velocity mode command. Motor runs at constant velocity. Parameters: Returns: None Raises: CallError on failure Example:
Hexfellow does not support VEL mode.

send_force_pos(pos, vlim, ratio)

Send force position mode command. Compliant position control with force ratio. Parameters: Returns: None Raises: CallError on failure Example:
RobStride, MyActuator, and Hexfellow do not support FORCE_POS mode.

Feedback Methods

request_feedback()

Request fresh feedback frame from motor. Parameters: None Returns: None Raises: CallError on failure Example:

get_state()

Get cached motor state from last received feedback. Parameters: None Returns: MotorState | None — Motor state or None if no feedback received Example:

CAN Configuration

set_can_timeout_ms(timeout_ms)

Set CAN communication timeout for this motor. Parameters: Returns: None Raises: CallError on failure Example:

Register Access (Damiao)

These methods are primarily for Damiao motors. See Register & Params Tutorial for register definitions and usage.

write_register_f32(rid, value)

Write 32-bit float value to register. Parameters: Returns: None Raises: CallError on failure Example:

write_register_u32(rid, value)

Write 32-bit unsigned integer value to register. Parameters: Returns: None Raises: CallError on failure Example:

get_register_f32(rid, timeout_ms=1000)

Read 32-bit float value from register. Parameters: Returns: float — Register value Raises: CallError on failure or timeout Example:

get_register_u32(rid, timeout_ms=1000)

Read 32-bit unsigned integer value from register. Parameters: Returns: int — Register value Raises: CallError on failure or timeout Example:

store_parameters()

Save current parameters to motor’s non-volatile memory. Parameters: None Returns: None Raises: CallError on failure Example:

RobStride-Specific Methods

These methods are only available for RobStride motors.

robstride_ping()

Ping RobStride motor to get device and responder IDs. Parameters: None Returns: tuple[int, int] — (device_id, responder_id) Raises: CallError on failure Example:

robstride_ping_host_id(host_id, timeout_ms=500)

Ping a RobStride motor using an explicit host-side ID. This host-id-specific path is used by the current scan flow when probing multiple possible feedback_id / host_id values. Parameters: host_id: int, timeout_ms: int = 500 Returns: tuple[int, int] — (device_id, responder_id) Raises: ValueError if host_id is outside 0..255; CallError on timeout or protocol failure Example:

robstride_get_param_f32_host_id(param_id, host_id, timeout_ms=1000)

Read a RobStride f32 parameter while forcing the host-side ID used for the request. This is primarily for exact scan/commissioning flows where several host IDs are probed. Parameters: param_id: int, host_id: int, timeout_ms: int = 1000 Returns: float Raises: ValueError if host_id is outside 0..255; CallError on failure or timeout Example:

robstride_set_device_id(new_device_id)

Set new device ID for RobStride motor. Parameters: Returns: None Raises: CallError on failure Example:

robstride_write_param_*

Write typed parameter values to RobStride motor. Example:

robstride_get_param_*

Read typed parameter values from RobStride motor. Example:

robstride_write_param_i8(param_id, value)

Write signed 8-bit RobStride parameter. Parameters: param_id: int, value: int Returns: None Raises: CallError on failure

robstride_write_param_u8(param_id, value)

Write unsigned 8-bit RobStride parameter. Parameters: param_id: int, value: int Returns: None Raises: CallError on failure

robstride_write_param_u16(param_id, value)

Write unsigned 16-bit RobStride parameter. Parameters: param_id: int, value: int Returns: None Raises: CallError on failure

robstride_write_param_u32(param_id, value)

Write unsigned 32-bit RobStride parameter. Parameters: param_id: int, value: int Returns: None Raises: CallError on failure

robstride_write_param_f32(param_id, value)

Write 32-bit float RobStride parameter. Parameters: param_id: int, value: float Returns: None Raises: CallError on failure

robstride_get_param_i8(param_id, timeout_ms=1000)

Read signed 8-bit RobStride parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: int Raises: CallError on failure or timeout

robstride_get_param_u8(param_id, timeout_ms=1000)

Read unsigned 8-bit RobStride parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: int Raises: CallError on failure or timeout

robstride_get_param_u16(param_id, timeout_ms=1000)

Read unsigned 16-bit RobStride parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: int Raises: CallError on failure or timeout

robstride_get_param_u32(param_id, timeout_ms=1000)

Read unsigned 32-bit RobStride parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: int Raises: CallError on failure or timeout

robstride_get_param_f32(param_id, timeout_ms=1000)

Read 32-bit float RobStride parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: float Raises: CallError on failure or timeout

Damiao Typed Param Methods

These methods provide typed parameter read/write paths for Damiao by param_id.

damiao_write_param_f32(param_id, value)

Write 32-bit float Damiao parameter. Parameters: param_id: int, value: float Returns: None Raises: CallError on failure

damiao_write_param_u32(param_id, value)

Write unsigned 32-bit Damiao parameter. Parameters: param_id: int, value: int Returns: None Raises: CallError on failure

damiao_get_param_f32(param_id, timeout_ms=1000)

Read 32-bit float Damiao parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: float Raises: CallError on failure or timeout

damiao_get_param_u32(param_id, timeout_ms=1000)

Read unsigned 32-bit Damiao parameter. Parameters: param_id: int, timeout_ms: int = 1000 Returns: int Raises: CallError on failure or timeout

Complete Example

See Also