Skip to main content
Source: bindings/python/README.md

motorbridge Python SDK

Channel Compatibility (PCAN + slcan + CAN-FD + Damiao Serial Bridge)

  • Linux SocketCAN uses interface names directly: can0, can1, slcan0.
  • For USB-serial CAN adapters, bring up slcan0 first: sudo slcand -o -c -s8 /dev/ttyUSB0 slcan0 && sudo ip link set slcan0 up.
  • CAN-FD transport is available both in CLI (--transport socketcanfd) and Python SDK (Controller.from_socketcanfd(...)), and is required for Hexfellow.
  • Damiao-only serial bridge transport is also available in CLI (--transport dm-serial --serial-port /dev/ttyACM0 --serial-baud 921600).
  • Full Damiao serial-bridge interface list and command patterns are documented in motor_cli/README.md (section 3.6 in motor_cli/README.zh-CN.md).
  • On Linux SocketCAN, do not append bitrate in --channel (for example can0@1000000 is invalid).
  • On Windows (PCAN backend), can0/can1 map to PCAN_USBBUS1/2; optional @bitrate suffix is supported.
Python binding layer on top of motor_abi.
Chinese version: README.zh-CN.md

README Navigation (What Each One Is For)

If this is your first time in this folder, read in this order:
  1. This file: README.md Purpose: Python binding overview (install, API scope, common commands).
  2. examples/README.md (English) / examples/READMEzh_cn.md (Chinese) Purpose: practical demo index and run instructions (from simplest to advanced). 2.5. ../motorbridge-docs Purpose: canonical Mintlify documentation site (tutorial + API style docs).
  3. get_started/README.md / get_started/README.zh-CN.md Purpose: pip-first onboarding path (install -> scan -> run).
  4. DAMIAO_PYTHON_REFERENCE.zh-CN.md Purpose: Damiao Python interface reference (parameter lookup style).
  5. DAMIAO_binding.md Purpose: Damiao binding implementation notes (design/internal behavior).
  6. README.zh-CN.md Purpose: Chinese overview for Chinese-speaking teammates.
Notes:
  • If your goal is “run something now”, start with Start Here (Simplest 2 Examples) in examples/README.md.
  • If your goal is CLI parameter lookup, see ../../motor_cli/README.md.

Scope

Packaging note:
  • Current package target version: 0.5.0.
  • Version checks are available through motorbridge.__version__, motorbridge.get_version(), and motorbridge-cli -v.
  • Published wheel includes motor_abi shared library and ws_gateway binary for that platform.
  • After pip install motorbridge, gateway binary path is typically: .../site-packages/motorbridge/bin/ws_gateway (or ws_gateway.exe on Windows).
  • Gateway launch command (added to PATH by pip):
    • motorbridge-gateway -- --bind 127.0.0.1:9002 ...
  • Security note:
    • keep loopback bind (127.0.0.1) for local usage.
    • if you bind to non-loopback addresses (0.0.0.0 or host IP), export MOTORBRIDGE_WS_TOKEN before launch.
    • clients must pass the token in x-motorbridge-token or Authorization: Bearer ....
  • macOS runtime note (only if you see dynamic library load errors):
    • Resolve binary path generically: GW="$(python3 -c "import motorbridge, pathlib; print(pathlib.Path(motorbridge.__file__).resolve().parent/'bin'/'ws_gateway')")"
    • Use package-local lib directory (no machine-specific absolute path): PKG_DIR="$(python3 -c "import motorbridge, pathlib; print(pathlib.Path(motorbridge.__file__).resolve().parent)")" DYLD_LIBRARY_PATH="$PKG_DIR/lib:${DYLD_LIBRARY_PATH:-}" "$GW" --bind 127.0.0.1:9002 --vendor damiao --channel can0 --model auto --motor-id 0x01 --feedback-id 0x11 --dt-ms 20
  • High-level API: Controller, Motor, Mode
  • CLI: motorbridge-cli
  • Controller constructors:
    • Controller(channel="can0") (SocketCAN/PCAN path)
    • Controller.from_socketcanfd(channel="can0") (CAN-FD path, required by Hexfellow)
    • Controller.from_dm_serial(serial_port="/dev/ttyACM0", baud=921600) (Damiao-only serial bridge)
  • Vendors:
    • Damiao: add_damiao_motor(...)
    • Hexfellow: add_hexfellow_motor(...)
    • MyActuator: add_myactuator_motor(...)
    • RobStride: add_robstride_motor(...)
    • HighTorque: add_hightorque_motor(...)
  • Unified state-query pattern:
    • Recommended flow: request_feedback() -> poll_feedback_once() -> get_state().
    • RobStride now supports this unified pattern via ABI-level compatibility (while robstride_ping() is still available).

Unified Mode Mapping Summary (Top-Level -> Vendor Native)

Note:
  • RobStride unified high-level control currently covers MIT / POS_VEL / VEL.
  • Torque/current is parameter-level only for RobStride (robstride_write_param_*), not a dedicated unified mode.
  • RobStride supports rs-00 through rs-06; pass the real model to add_robstride_motor(...) because parameter read/write uses the common section 4 runtime parameter table.
  • RobStride feedback/host default should use 0xFD; scan tries 0xFD,0xFF,0xFE,0x00,0xAA by default.
  • RobStride feedback_id / host_id is not the motor device_id; scan hits report the motor ID as probe / device_id.

Quick Start

Damiao over serial bridge:
RobStride quick use:
MyActuator quick use:
Hexfellow quick use (CAN-FD only):

CLI Examples

Damiao:
RobStride:
Use the actual RobStride model (rs-00 … rs-06) in Python CLI and SDK calls. The same control methods are available across the series, but manual parameter IDs and data types are selected from that model. RobStride MIT and POS_VEL quick checks:
RobStride parameter read:
Damiao parameter read/write:
Unified scan (all vendors):
RobStride-focused scan and ID update:
HighTorque via binding:
HighTorque via Rust CLI:

Experimental Windows Support (PCAN-USB)

Linux remains the primary target. Windows support is experimental and currently uses PEAK PCAN.
  • Install PEAK PCAN driver + PCAN-Basic runtime (PCANBasic.dll).
  • Use channel as can0@1000000 (maps to PCAN_USBBUS1 at 1Mbps).
Recommended quick validation with Rust CLI on Windows:
Local wheel build (Windows):

Example Programs

  • Damiao wrapper demo: examples/python_wrapper_demo.py
  • Hexfellow CAN-FD demo: examples/hexfellow_canfd_demo.py (MIT / POS_VEL only)
  • Damiao maintenance demo: examples/damiao_maintenance_demo.py
  • Damiao register rw demo: examples/damiao_register_rw_demo.py
  • Damiao dm-serial demo: examples/damiao_dm_serial_demo.py
  • RobStride wrapper demo: examples/robstride_wrapper_demo.py
  • Full Damiao mode demo: examples/full_modes_demo.py
  • Damiao scan / tune / position helpers:
    • examples/scan_ids_demo.py
    • examples/pid_register_tune_demo.py
    • examples/pos_ctrl_demo.py
    • examples/pos_repl_demo.py
See examples/README.md (English) or examples/READMEzh_cn.md (Chinese).

Damiao Full-Coverage Status

Damiao usage in Python examples is now covered end-to-end:
  • control modes: mit / pos-vel / vel / force-pos
  • transport paths: SocketCAN/PCAN constructor + from_dm_serial(...)
  • maintenance ops: clear_error, set_zero_position, set_can_timeout_ms, request_feedback
    • project guard for Damiao set-zero: call disable() before set_zero_position()
    • no user-facing ms parameter for set-zero; core applies fixed 20ms settle
  • register APIs: get/write f32, get/write u32, store_parameters

End-to-End Demo Commands

Notes

  • id-dump is a Damiao workflow; id-set supports Damiao and RobStride; scan supports damiao|hexfellow|myactuator|robstride|hightorque|all.
  • For RobStride id-set, --new-motor-id changes device_id; --feedback-id remains the host-side ID.
  • RobStride motor_id / device_id is validated as 1..255; feedback_id / host_id is validated as 0..255 to prevent silent ctypes truncation.
  • RobStride scan probes each --feedback-ids host_id exactly through host-id-specific ABI helpers; invalid host IDs are rejected instead of silently falling back.
  • Mode.MIT and send_force_pos are not available for MyActuator in ABI wrapper.
  • Hexfellow supports MIT and POS_VEL through ABI wrapper; VEL and FORCE_POS return unsupported.
  • Full Damiao tuning reference stays in:

PyPI Auto Publish (GitHub Actions)

This repository includes .github/workflows/pypi-publish.yml.
  • Tag publish policy:
    • push vX.Y.Z -> publish the same artifacts to both TestPyPI and PyPI
  • Manual publish is still available via workflow Python Publish:
    • testpypi (only TestPyPI)
    • pypi (only PyPI)

One-time setup (token mode)

  1. Create API token on PyPI and add repository secret PYPI_API_TOKEN.
  2. Create API token on TestPyPI and add repository secret TEST_PYPI_API_TOKEN.
  3. Keep package version unique for every upload (for example 0.1.6, 0.1.7).